Technical FAQs

Ask a Question

What are the repair parts for the H362DX, series E1 (may be shown as E01)?

Issue:
Repair parts

Product Line
:
Heavy Duty Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The repair parts for the H362DX, series E1 (E01) are as follows. No other parts are available.
-Interior Assembly - 9422TD3 (includes the line and load base, mechanism and operating rod)
-Handle Assembly - NF200
-Enclosure Mounting Foot - 0201847 (4 total required)



CTA-ID : 15797
Was this helpful?
What can we do to improve the information ?