Technical FAQs

Ask a Question

Does Square D offer Type 4X Safety Switches rated at 800A or 1200A?

Issue:
Application

Product Line:
Heavy Duty Safety Switch

Environment:
Selection

Cause:
Selection

Resolution:
We do offer Type 4X safety switches in Type 304 or Type 316 stainless steel enclosures, but only through 600A. We also offer Type 4X safety switches in fiberglass reinforced polyester enclosures through 200A.
Was this helpful?
What can we do to improve the information ?