Technical FAQs

Ask a Question

Is the L600AWK UL Listed?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Environment:
Selection

Cause:
Selection

Resolution:
Yes, it is. File E-136861.
Was this helpful?
What can we do to improve the information ?