Technical FAQs

Ask a Question

What is the lug wire range for the PKOGTA4?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Environment:
Selection

Cause:
Selection

Resolution:
The PKOGTA4 will accept up to (4) #6 AWG - 250 KCMIL (AL or CU) ground wires.
Was this helpful?
What can we do to improve the information ?