Technical FAQs

Ask a Question

What is a L600AWKMC?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Environment:
Selection

Cause:
Selection

Resolution:
The L600AWKMC is offered for use with the L Frame PowerPact Molded Case Switch. The enclosure is listed and labeled as Rainproof and Dusttight and is suitable for Type 1, 3, 3R, 5 or 12 installations. When used in an outdoor, rainproof application, remove the drain screw in the bottom endwall and discard.
Was this helpful?
What can we do to improve the information ?