Technical FAQs

Ask a Question

What is the difference between the Trace SWI and SWI/PAR?

Trace SW Stacking Cables Differences 


Here is the pin out  for the Series Stacking Cable 
This is used for 120/240V output











Here is the pin out for the Parallel Stacking Cable.
This is used in conjunction with SWI/PAR parallel stacking transformer (120V at 2 times current rating)









IMPORTANT : SWI/PAR requires external parallel stacking transformer (see attached)





Was this helpful?
What can we do to improve the information ?