Technical FAQs

Ask a Question

What is the XC540-NA output when power factor is unity?

 
What is the XC540-NA output when power factor is unity?





 
 
 
The XC540-NA is rated as 540KVA over +/-0.80 Power Factor Range.
 
So, at Unity Power Factor , its  AC output is 540KW.
 
At +/- 0.80 PF, its Active Power Output is 432KW and Reactive Power Output is +/- 324 KVAR.
 
Please note that all these figures are at Inverter Terminals.
 
Generally, there are both Active & Reactive Power loss in the collector system including the Transformer loss between the  Inverter & Point of Interconnection ( POI ).
 
These losses need to be considered for true output at POI.
 
The attached  information will provide additional information/ clarification.
 
Was this helpful?
What can we do to improve the information ?