Technical FAQs

Ask a Question

What is the difference between ZBVG6 and ZBVG65 Light Modules?

Issue:
What is the difference between ZBVG6 and ZBVG65?

Product line:
XB4 & XB5 22mm Pushbuttons.

Environment:
Light module

Cause:
A need to know difference between two similar light module part numbers.

Resolution:
ZBVG6 light module has standard screw terminal feature whereas the  ZBVG65 light module,  has spring clamp terminal feature
Was this helpful?
What can we do to improve the information ?