Technical FAQs

Ask a Question

Where is the blank for the last meter column located when joining MC43L, MC43L3, MC43L200B, MC443LB in the meter stacks?

Issue:
For MC43, MC43L3, MC43L200B, MC443LB, where is the blank for the last meter column?

Product Line:
Canadian Meter centers up to 240V

Cause:
Each meter center column has side holes to connect the bus bars between one column to another, there is a blank required to cover the hole in the last column.

Resolution:
The blank plate is bolted in th tap box. Customer needs to remove this blank plate from the tap box and after install it in the last meter column.
Was this helpful?
What can we do to improve the information ?