Technical FAQs

Ask a Question

QO Tandem breaker with push-in connections 1960-1961

Issue:
QO Tandem breaker with push-in connections 1960-1961

Product Line:
Electrical Distribution

Environment:
QO Tandem

Cause:
History

Resolution:
QO Tandem was originally introduced with push-in connections in 1960, then the push-in connection was dropped in 1962.  No catalog number changes to the product when this change occurred.

QO Tandem  QO1515 and QO2020 were introduced with push-in connections in the 1960 digest with availability to be announced in June 1960.  The push-in connections were also advertised in the 1961 digest, but not in 1962.  I am assuming at this point that in 1962 the push-in connections were changed to a screw connection that we see today.

Was this helpful?
What can we do to improve the information ?