Technical FAQs

Ask a Question

What is the size of the conductors that come with the NQMB2Q kit?

Issue:
Parts in main breaker kit

Product Line:
Panelboards

Environment:
NQ

Cause:
Wire size

Resolution:

 
 
 
 There are three 80110-327-03 cables which are 4/0 copper XHHW , 6.63" L and stripped back 1.25" at the ends
 
Was this helpful?
What can we do to improve the information ?