Technical FAQs

Ask a Question

Can the Canadian INDOOR(NEMA 1) Homeline Loadcentres be installed horizontally or on their sides?

Issue:
Installing Canadian INDOOR (NEMA 1) Homeline loadcentres Horizontally.

Product Line:
Canadian INDOOR Homeline Loadcentres

Environment:
installation of Canadian INDOOR ONLY Homeline loadcentres

Cause:
Installing loadcentres in a horizontal position. 

Resolution:
In Canada the installation of a INDOOR(NEMA 1) Loadcentre is determined by the local code authority having jurisdication and not by Square D.
Was this helpful?
What can we do to improve the information ?