Technical FAQs

Ask a Question

What is the recommended replacement for the ATV56 drives?

Issue:
What is the recommended replacement for the ATV56 drives?

Product Line:
ATV56

Environment:
All

Cause:
Obsolete

Resolution: 
The old ATV56 was a variable torque only drive so the ATV61 family will be a suitable replacement.  If the old drive was mounted on top of a BeleBox set up then you may need to add the extended I/O option card VW3A3201 to wire up your status LED.

Call the Drives Product Support Group at 1888 778 2733 if you have any question.
Was this helpful?
What can we do to improve the information ?