Technical FAQs

Ask a Question

Is H461 CSA Certified?

Issue:
Standards

Product Line:
Heavy Duty Safety Switch

Environment:
Standards certification

Cause:
Assurance of standards met

Resolution:
Yes, H461 is CSA Certified as well as UL Listed. Both CSA and UL marks are applied to the wiring diagram.
Was this helpful?
What can we do to improve the information ?