Technical FAQs

Ask a Question

Can a 225Amp main breaker be installed in the CHOM2040M200GC loadcentre?

Issue:
installation of a 225Amp main breaker

Product Line:
Canadian Homeline Loadcentres

Environment:
Applies to Canadian Homeline Loadcentres CHOM2040M200GC, CHOM3060M200GC, CHOM4284M200GC, CHOM60120M200GC

Cause:
Increase the main breaker rating

Resolution:
The CHOM2040M200GC is ONLY rated 200amp Maximum and a 225amp main breaker CANNOT be installed.

Was this helpful?
What can we do to improve the information ?