Technical FAQs

Ask a Question

Can a 225Amp main breaker be installed in the CHOM4284M200GC loadcentre?

Issue:
Mains rating for the CHOM4284M200GC loadcentre?

Product Line:
Canadian Homeline Loadcentres

Environment:
Maximum Ampere rating for the loadcentre

Cause:
Increase ampere rating of the main breaker

Resolution:
NO, the CHOM4284M200GC is rated 200amp Maximum and a 225amp main breaker CANNOT be used.
Was this helpful?
What can we do to improve the information ?