Technical FAQs

Ask a Question

XW AGS shuts down shortly after auto-start.

XW AGS shuts down shortly after auto-start



Verify generator is not supplying AC1 input. Otherwise the generator will shut down due to "AC in GOOD", which occurs
once the grid is restored. XW AGS is designed around AC2 input. Certain functions do not apply to AC1, such as
Gen Cool Down. It is also important the customer does not inadvertently sell power back to the generator.
Was this helpful?
What can we do to improve the information ?