Technical FAQs

Ask a Question

What are the repair parts for a HOM12M200PRB, Series S04, load center?

Issue:
current design repair parts

Prouduct line:
Homeline load centers

Environment:
repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable.
Cover - 4056317650 (Includes hinges attached to left side of cover) 
Cover Mounting Screw - 2142217101 (2 Required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim with Labels - 4056354401K
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - HOM12M200PRBI (interior assembly does not include main breaker, see main breaker below)
Main Breaker - QOM2200VH
Neutral Bonding Screw - 4028345850K
Note: Covers do not have labels applied.

Was this helpful?
What can we do to improve the information ?