Technical FAQs

Ask a Question

What are the repair parts for a HOM3060M100PC, Series S04 load center?

Issue:
Current design repair parts

Product Line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:
Cover - HOMC30U125C
Cover Mounting Screw - 4020513002K (6 required)
Cover Door Hinge - 4028356450K
Door Latch Kit - 4020284450K
Interior Assembly - HOM3060M100PCI (Interior assembly does not include the main breaker, see main breaker below)
Neutral Bonding Screw - 4028345850K
Main Breaker - QOM100VH

Was this helpful?
What can we do to improve the information ?