Technical FAQs

Ask a Question

Is it possible and allowed to connect two or more handles XY2AU to one safety module XPSVC?

Issue:
Is it possible and allowed to connect two or more handles XY2AU to one safety module XPSVC?

Product Line:
Enabling switch

Environment:
XY2AU

Cause:
Is it possible and allowed to connect two or more handles XY2AU to one safety modules XPSVC?

Resolution:
This is not recommended.
The XPSVC unit can monitor only 1 XY2AU* enabling switch.
Was this helpful?
What can we do to improve the information ?