Technical FAQs

Ask a Question

What is included in the value pack HOM3060M200PC1AVP?

Issue:
Determining value pack components

Product Line:
Homeline load centers

Environment:
Breakers and load center included in value pack

Cause:
component parts

Resolution:
It includes;
(1) HOM3060M200PC (Homeline plug-on neutral, 200Amp, 30space- 60 circuit maximum, indoor, main breaker load center), 
(1) HOM115PCAFI (HOM, Plug-on Neutral, 15 A, single-pole Combination Arc Fault branch circuit breaker.
(3) HOM120 (Homeline 20 A single-pole branch circuit breaker)
(2) HOM230 (Homeline 30 A, double-pole branch circuit breaker)
Was this helpful?
What can we do to improve the information ?