Technical FAQs

Ask a Question

Can I set my XW multi-unit system to trigger AUX ports at different voltages?

 Can I set my XW multi-unit system to trigger AUX ports at different voltages?




When multi-unit systems are set for the same trigger type (i.e. Low Battery Voltage), the voltages cannot be different.
It is possible to set different trigger types, such as High Battery V, Fault, Lo/Hi Batt temp. 
If customer has MPPT controllers, they can be set to same trigger type and different voltage from inverter system. 
Remember MPPT80 does not output voltage (dry relay contacts only).




Was this helpful?
What can we do to improve the information ?