Technical FAQs

Ask a Question

What drive product line replaces the obsolete ATV58?

Issue:
What drive product line replaces the obsolete ATV58?

Product Line:
Altivar 58 ATV58

Environment:
All models

Cause:
Cross reference

Resolution:
The ATV58 was a full feature VFD rated for variable torque and constant torque loads.  Replace or cross reference the ATV58 with:

ATV600 series for variable torque loads
ATV71 for constant torque loads

Was this helpful?
What can we do to improve the information ?