Technical FAQs

Ask a Question

How is a run permissive function added to an ATV61/71?

Issue:
How is a run permissive function added to an ATV61/71?

Product Line:
Altivar 61 71 ATV61 ATV71

Environment:
All models

Cause:
The VFD needs to be disabled unless a condition is met.

Resolution:
This function is typically done with a logic input assigned to freewheel stop: 
Menu, Application Function
Sub-menu, Stop Configuration
Parameter, Freewheel Stop Assign

When the logic input is low, the VFD is in a disabled freewheel stop mode, whether in Local or Remote modes of operation.  Drive status is NST.
When the logic input is high, the VFD is permitted to run, but will require a run command to start.
Was this helpful?
What can we do to improve the information ?