Technical FAQs

Ask a Question

What is the torque value for the wire binding screws on PK15GTA?

Issue:
Torque

Product Line:
Ground Bars

Environment:
Ground Bar Torque

Cause:
Assuring proper torque applied to connections

Resolution:
#14 - #10 CU, #12 - #10 AL = 20 Lb.In.
#8 CU/AL = 25 Lb.In.
#6 - #4 CU/AL = 35 Lb.In.
Two #14 - #12 CU, Two #12 - #10 AL = 25 Lb.In.
Was this helpful?
What can we do to improve the information ?