Technical FAQs

Ask a Question

Is HU466 CSA Certified?

Issue:
Standards

Product Line:
Heavy Duty Safety Switch

Environment:
4 pole safety switch

Cause:
Assurance of standards met

Resolution:
No, it does not carry a CSA mark. It is UL Listed and carries the UL mark. For a CSA Certified equivalent, consider using a CHU466.
Was this helpful?
What can we do to improve the information ?