Technical FAQs

Ask a Question

Are the ATV212 drives Marine Lloyd's certified?

Issue:
Marine Lloyd's Certificate for the ATV212 drive

Product Line:
ATV212

Environment:
All models and serial numbers

Cause:
None

Resolution:
No, the only drive we have Marine Lloyd's certified is the ATV71H. 
Drive certificates can be downloaded form the following link:
http://www.schneider-electric.com/products/us/en/50000-ac-drives-and-soft-starts/50010-ac-variable-torque/60162-featured-altivar-212-ac-drive/

Was this helpful?
What can we do to improve the information ?