Technical FAQs

Ask a Question

What is the horsepower (HP) rating of a H367N, H367NR or H367NAWK safety switch?

Issue:
Ratings

Product Line:
Heavy Duty Safety Switch

Environment:
Horspower Ratings

Cause:
Selection criteria

Resolution:
The H367N, H367NR and H367NAWK HP ratings are: 200 HP @ 480Vac or 250 HP @ 600Vac if using fast acting fuses. 500 HP @ 480Vac or 600Vac is using time delay fuses. 50 HP @ 250Vdc or 600Vdc.

Was this helpful?
What can we do to improve the information ?