Technical FAQs

Ask a Question

What is included in the value pack HOM4080M200PC1AVP?

Determining value pack components

Product Line:
Homeline load centers

Breakers and load center included in value pack

component parts

It includes;
(1) HOM4080M200PC (Homeline plug-on neutral, 200Amp, 40space- 80 circuit maximum, indoor, main breaker load center), 
(1) HOM115PCAFI (Homeline, 15 A, single-pole, Plug-On Neutral, Combination Arc Fault Breaker)
(3) HOM120 (Homeline 20 A single-pole branch circuit breaker)
(2) HOM230 (Homeline 30 A, double-pole branch circuit breaker)
Was this helpful?
What can we do to improve the information ?