Technical FAQs

Ask a Question

What are the repair parts for a HOM4080L225PRB, Series S04 load center?

Current design repair parts
Product Line:
Homeline load centers
Repair parts

Only the parts listed below are considered field replaceable.
Cover - 4056317250  (Includes hinges attached to left side of cover)
Cover Mounting Screw - 2142217101 (2 Required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure) 
Interior Trim with Labels - 4056314201K   
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - HOM4080L225PRBI (interior assembly does NOT include the main lugs, see below main lugs)
Main Breaker - QOL225
Neutral Bonding Screw - 4028345850K
Note: Covers do not have labels applied.
Was this helpful?
What can we do to improve the information ?