Technical FAQs

Ask a Question

What is included in the value pack HOM1224L125PGCVP?

Issue:
Determining value pack components

Product Line:
 Homeline load centers

Environment:
Breakers and load center included in value pack

Cause:
component parts

Resolution:
It includes the following:
(1) HOM1224L125PGC (a Homeline plug-on neutral, 125A max, 12space- 24 circuit, indoor, main lug load center with a ground bar that has 15 holes and a 2/0 max. Lug).  
(2) HOM120 (Homeline 20 A single-pole circuit breakers).
 
Was this helpful?
What can we do to improve the information ?