Technical FAQs

Ask a Question

What are the repair parts for a HOM816L125PC, Series S04 load center?

Issue:
current design repair parts

Prouduct line:
Homeline load centers

Environment:
repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable:
Cover - HOMC12UC
Cover Mounting Screw - 4020513002K
Cover Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit 4020284450K
Interior Assembly - HOM816L125PCI (interior assembly does not include the main lugs, see main lug kit below)
Neutral Bonding Screw - 4028345850K
Main Lugs - QOL125

Was this helpful?
What can we do to improve the information ?