Technical FAQs

Ask a Question

How is the Ground-Fault Interface Module powered?

Issue:
How is the Ground-Fault Interface Module, S48891, powered?

Product Line:
S48891, Powerpact P, Powerpact R , Masterpact NT, Masterpact NW, and Compact NS630B-1250
 
Resolution:
The unit is powered through the Micrologic trip unit.
 
Was this helpful?
What can we do to improve the information ?