Technical FAQs

Ask a Question

Can a QO or HOMELINE load center be used on a 250Vdc system?

Issue:
Application

Product Line:
QO and HOMELINE

Environment:
QO and HOMELINE load centers

Cause:
Application at 250Vdc

Resolution:
No, neither QO nor HOMELINE load centers can be used on a 250Vdc system. Consider using an I-Line or QMB panel board for the 250Vdc application.

Was this helpful?
What can we do to improve the information ?