Technical FAQs

Ask a Question

Will a QOB40MW200-2 accept either QO tandem breakers or QOT tandem breakers?

Issue:
Application

Product Line:
QO load center

Environment:
Tandem breaker

Cause:
Selection of correct breakers

Resolution:
QOB40MW200-2 was merely a box number, not the load center number. It was associated with the load center catalog number QO3040MW200, which would accept up to 10 QOT tandem circuit breakers.
Was this helpful?
What can we do to improve the information ?