Technical FAQs

Ask a Question

Will a QOB40MW150-1 accept either QO tandem breakers or QOT tandem breakers?

Issue:
Application

Product Line:
QO load center

Environment:
Tandem breaker

Cause:
Selection of correct breakers

Resolution:
QOB40MW150-1 was merely a box number, not the load center number. It was associated with the load center catalog number QO30MW150VH, which would not accept QOT tandem circuit breakers. Although the QO tandems would physically fit, they could not legally be used since the QO30MW150VH was a Class CTL load center.
Was this helpful?
What can we do to improve the information ?