Technical FAQs

Ask a Question

Can a door be field installed on the cover of a QO612L100F load center?

Issue:
load center cover and door

Product line:
QO load centers

Environment:
QO612L100F load center cover

Cause:
The QO612L100F load center cover comes standard without a door

Resolution:
The QO612L100F comes with a cover that does NOT include a door. The cover with a door is part number 4055345250. BUT the cover does not include any labels. It would be less expensive and faster for a customer to order the complete load center that comes with a cover and door and they will obtain all the correct labeling.
Was this helpful?
What can we do to improve the information ?