Technical FAQs

Ask a Question

HOM-CAFI Padlock Attachment

Issue:
What is the padlock attachment for an HOM-CAFI breaker?

Product Line
Homeline Circuit Breakers 

Environment:
HOM-CAFI Breakers and accessories

Cause:
Need to lock a CAFI breaker in the off position

Resolution:
The HOMELEC1PA is for locking the single pole HOM-CAFI, HOM-PCAFI, HOM-EPD, HOM-GFI, HOM-DF and HOM-PDF breakers in the on or off position.
The HOMELEC2PALA is for locking the two pole HOM-CAFI, HOM-EPD, and HOM-GFI breakers in the on or off position.
Was this helpful?
What can we do to improve the information ?