Technical FAQs

Ask a Question

Conext RL "qualified person" password

 Conext RL "qualified person" password



1. If you are in the start-up menu of the inverter, the password is presseing SEL+ENT buttons together for more than 10 seconds. We acknowledge the gap in the manual. The below erratum is inserted with every product shipped and is listed on our website.
 
If you are in that part of flowchart to set Inverter ID, the password is: "SEL+ENT>3seconds"
 
2. If you are using the Conext RL Config tool software, the password for Installer Access is: ConextRL
 
Was this helpful?
What can we do to improve the information ?