Technical FAQs

Ask a Question

Is the ATS01 rated Class 1 Division 2?

Issue:
Is the ATS01 rated Class 1 Division 2?

Product Line:
ATS01

Environment:
All models and serial numbers

Cause:
None

Resolution:
Class 1 Locations are made hazardous by the presence of flammable gases, liquids or vapors.  Because these electrical devices can arc they are not rated for Class 1 Division 2.

Was this helpful?
What can we do to improve the information ?