Technical FAQs

Ask a Question

What is the catalog number HOM2040M200PTBP and what does it consist of?

Issue:
Determining bulk pack components

Product Line:
Homeline load centers

Environment:
Bulk pack contents

Cause:
component parts

Resolution:
The HOM2040M200PTBP is a Homeline, Plug-On Neutral, 200amp, 20space-40circuit, NEMA 1(indoor) Main Breaker load center. This catalog number is a BULK PACK quantity of 27 load centers, LESS the standard cover and carton(cardboard box). This load center was set up specifically for Manufactured Housing customers who use the WHITE covers. Customers can obtain this bulk pack quantity of load centers without the standard gray covers and obtain the white covers separately.
Was this helpful?
What can we do to improve the information ?