Technical FAQs

Ask a Question

What is the maximum size of wire that can be used in the P1200R circuit breaker enclosure?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Environment:
M Frame

Cause:
Clarification

Resolution:
This enclosure is marked for use with 500 KCMIL conductors maximum.
Was this helpful?
What can we do to improve the information ?