Technical FAQs

Ask a Question

Is the ATV61 offered with an IP54 enclosure rating?

Issue:
Is the ATV61 offered with an IP54 enclosure rating?

Product Line:
Altivar 61 ATV61

Environment:
ATV61W .....

Cause:
None

Resolution:
The ATV61W...N4U models are Nema 12 / IP54 rated.  These are 400/480V models only. 
This offering was discontinued end of 2015.
Consider the ATV600 series Process Drive options.
Was this helpful?
What can we do to improve the information ?