Technical FAQs

Ask a Question

What are the ratings for the 250A DC disconnect in the XW PDP?

XW 250A DC Disconnect Information 

@ 80Vdc -> Ics= 10000A / Icu 25000A
@ 160Vdc -> Ics=  5000A / Icu 10000A
In : 250A
Vimp 4KV
Trip Current: 313A
Max V: 160V
AIC: 10000A
Was this helpful?
What can we do to improve the information ?