Technical FAQs

Ask a Question

What size of circuit breaker should be used to feed the EV230WS EVSE?

Issue:
Applicaition

Product Line:
EVSE

Environment:
Application

Cause:
Feed with correct circuit breaker

Resolution:
The circuit should be fed by a 40 ampere/2 pole circuit breaker, non-GFI and #8 AWG wire should be used.
Was this helpful?
What can we do to improve the information ?