Technical FAQs

Ask a Question

XW AGS with Combox - State/Reason/Action code listing

 XW AGS with Combox - State/Reason/Action code listing




AGS Operating State
Device State can report one of the following values:

• 0=Hibernate
• 1=Power Save
• 2=Safe Mode
• 3=Operating
• 4=Diagnostic Mode
• 5=Remote Power Off
• 255=Data Not Available
 

Generator State
Auto Generator State can report one of the following values:

• 0=Quiet Time
• 1=Auto On
• 2=Auto Off
• 3=Manual On
• 4=Manual Off
• 5=Gen Shutdown
• 6=Ext Shutdown
• 7=AGS Fault
• 8=Suspend
• 9=Not Operating
 

Generator Actions
Auto Generator Action can report one of the following values:

• 0=Preheating
• 1=Start Delay
• 2=Cranking
• 3=Starter Cooling
• 4=Warming Up
• 5=Cooling Down
• 6=Spinning Down
• 7=Shutdown Bypass
• 8=Stopping
• 9=Running
• 10=Stopped
• 11=Crank Delay
 

Generator On Reason

• 0=Not On
• 1=DC Voltage Low
• 2=Battery SOC Low
• 3=AC Current High
• 4=Contact Closed
• 5=Manual On
• 6=Exercise
• 7=Non Quiet Time
• 8=Ext On via AGS
• 9=Ext On via Gen
• 10=Unable To Stop
• 11=AC Power High
• 12=DC Current High
 

Generator Off Reasons

• 0=Not Off
• 1=DC Voltage High
• 2=Battery SOC High
• 3=AC Current Low
• 4=Contact Opened
• 5=Reached Absorp
• 6=Reached Float
• 7=Manual Off
• 8=Max Run Time
• 9=Max Auto Cycle
• 10=Exercise Done
• 11=Quiet Time
• 12=Ext Off via AGS
• 13=Safe Mode
• 14=Ext Off via Gen
• 15=Ext Shutdown
• 16=Auto Off
• 17=Fault
• 18=Unable To Start
• 19=Power Low
• 20=DC Current Low
• 21=AC Good
 


AGS Fault Status
Fault Bitmap 0 can report one or more of the following values:

• bit0=F69:Node Instance Duplicated
• bit1=F200:Exceeded max number of start tries
• bit2=F201:Unable to stop gen
• bit3=F203:Gen Stopped by ext sensor
• bit4=F500:Serial Number Failure
• bit5=F501:Memory Failure
• bit6=F505:Internal Failure
 

AGS Warning Bits
Warning Bitmap 0 can report one or more of the following values:

• bit0=W200:Generator was stopped manually
• bit1=W201:Generator was started manually
• bit2=W202:Unable to start generator
• bit3=W203:Manual Off
• bit4=W204:Max Genset Cycle with no user intervention
• bit5=W205:Generator started by its switch
• bit6=W206:Mismatched triggers
• bit7=W207:Mismatched triggers
• bit8=W208:Automatic start and stop triggers not enabled
• bit9=W209:Generator external stop
• bit10=W250:Value failed to change
• bit11=W500:Network connection lost
• bit12=W501:Memory problem - cleared memory
• bit13=W599:Invalid Associations


Was this helpful?
What can we do to improve the information ?