Technical FAQs

Ask a Question

What is the material of ZBZ41?

What is the material of ZBZ41 mounting adapter to mount 22mm operators in 30mm holes?

Product Line:
Control operators

Applies to XB4, XB5, ZB4 and ZB5 operators

Customer wants to know the material the ZBZ41 adaptor is made from, and if it is availabe in stainless steel?

It is made of metal, not available in stainless steel
Was this helpful?
What can we do to improve the information ?