Technical FAQs

Ask a Question

What is the HP size of a FLEX58D33N4?

Issue:
What is the HP size of a FLEX58D33N4?

Product Line:
FLEX58

Environment:
FLEX58D33N4

Cause:
Is this a 30HP or 40HP drive?

Resolution:
This drive is dual rated:
30HP for a constant torque load
40HP for a variable torque load
Was this helpful?
What can we do to improve the information ?