Technical FAQs

Ask a Question

Are the main breakers provided in the QO1DM10020TRBR Generator Panel?

Issue:
Product characteristics

Product Line:
QO Load Center

Environment:
Generator panels

Cause:
Clarification

Resolution:
Yes, the QO1DM10020TRBR will include a QO2100 backfed main breaker (100A for the utility feed) and a QO220 backfed main breaker (20A for the generator feed). The two breakers will be interlocked so that only one can be energized.
Was this helpful?
What can we do to improve the information ?