Technical FAQs

Ask a Question

Do QO and Homeline load centers come with the branch breakers already installed?

Issue:
Product features

Product Line:
QO and HOMELINE Load Centers

Environment:
Factory modifications

Cause:
Define product features

Resolution:
Branch breakers must be ordered separately and field installed into the load center. A selcct few load centers are offered as "Value Packs", which will include a select few branch breakers, but the breakers will not be installed.
Was this helpful?
What can we do to improve the information ?